Galco will be closed Friday, July 3, for Independence Day.

Create or sign in to your account for the best pricing!

Your account pricing is now applied.

Toggle Nav
Search
My Cart

Terminal Strip

We can't find products matching the selection.

Industrial Terminal Strips for Reliable Panel Wiring and Circuit Organization

Industrial terminal strips provide a secure, serviceable way to terminate and distribute conductors inside control panels, junction boxes, and industrial equipment. Instead of splicing wires or landing multiple conductors under a single device terminal, terminal strips help maintenance and build teams organize circuits, simplify troubleshooting, and support safe modifications over the life of the system. On this page, Galco's terminal strip category sits within the broader terminal blocks lineup, an essential foundation for clean industrial wiring practices.

For correct selection, start with the electrical and mechanical requirements: conductor size range (wire gauge), current/voltage ratings, and termination method (screw, clamp/spring, etc.) that matches your facility's wiring standards and technician workflow. Also consider how the terminal strip will be mounted and expanded. For many industrial control builds, DIN rail terminal solutions make it easier to add circuits, keep consistent spacing, and maintain a structured layout. If your application involves equipment-level electronics or board-level connections rather than panel wiring, you may also want to compare with PCB mount options within the same terminal blocks family.

Correct usage is about durability and maintainability: label terminals clearly, apply consistent torque (where applicable), and plan for strain relief and bend radius so conductors aren't stressed at the termination point. Many issues blamed on "bad terminals" are actually caused by loose connections, conductor mismatch, or poor mechanical support. When you're building out terminal rows, the right accessories help protect and stabilize the assembly; items like end stops and end plates can improve safety and keep terminal groups aligned, while broader terminal block accessories support consistent, service-friendly panel standards.

Frequently Asked Questions

What is a terminal strip used for in an industrial control panel?

A terminal strip is used to land field wiring and internal panel wiring in an organized, serviceable way, making it easier to commission equipment, isolate circuits for troubleshooting, and perform maintenance without cutting/splicing conductors. They're especially useful when multiple field devices terminate in the same enclosure, or when wiring needs to be grouped by function (power, control, signals). If you're standardizing panel builds, it's often helpful to start at the terminal blocks level and then choose the terminal strip style that fits the application.

How do I choose the right terminal strip size and rating?

Match the terminal strip to your conductor size range, required current/voltage, and the environment inside the enclosure (heat, vibration, and service access). Also consider how many circuits you need now, and how many you'll likely add later, so you don't paint yourself into a corner with an undersized layout. For modular, expandable designs, DIN rail terminal blocks are a common industrial approach because they're easier to reconfigure as equipment changes.

What accessories are important when installing terminal strips?

Accessories help with both safety and uptime. End-of-row hardware like end stops can prevent terminals from shifting on a rail, while end plates help cover exposed ends and support clearer grouping. Depending on your panel standards, additional terminal block accessories can improve labeling, jumpers/bridging, and overall serviceability, reducing troubleshooting time for plant maintenance teams.