Galco will be closed Friday, July 3, for Independence Day.

Create or sign in to your account for the best pricing!

Your account pricing is now applied.

Toggle Nav
Search
My Cart

Soft Starters

We can't find products matching the selection.

Soft Starters for Controlled Motor Starting and Reduced Inrush Current

Soft starters are used to gradually ramp the voltage to an electric motor during startup, reducing inrush current and mechanical stress compared with across-the-line starting. By controlling acceleration and, in many applications, deceleration, soft starters help protect motors, couplings, belts, pumps, conveyors, and connected equipment from sudden torque changes.

In industrial automation and control systems, soft starters are commonly used with pumps, fans, compressors, conveyors, mixers, crushers, and other motor-driven equipment where smooth starting is important. They help reduce electrical demand during startup, limit voltage dips, and minimize mechanical shock on driven loads.

Soft starters are especially useful in applications where the motor does not require continuous speed variation after startup. Unlike variable frequency drives, which control motor speed during operation, soft starters are primarily used to manage motor starting and stopping. This makes them a strong fit for fixed-speed motor applications where reduced starting current, controlled acceleration, and equipment protection are the main priorities.

Soft starter accessories can support installation, configuration, and long-term reliability by helping adapt the starter to the control panel, motor circuit, or operating environment. Depending on the system, accessories may include items for mounting, communication, operator interface, wiring, protection, or replacement. Selecting the correct accessories helps ensure the soft starter is properly integrated with the motor control system.

When selecting a soft starter, key considerations include motor horsepower, voltage, full-load current, starting duty, ramp time, bypass configuration, overload protection, enclosure requirements, and load type. Proper selection helps improve motor reliability, reduce downtime, and extend the service life of connected mechanical and electrical components.

Frequently Asked Questions

What types of motors can use soft starters?

Soft starters are most commonly used with three-phase AC induction motors. The soft starter must be selected to match the motor voltage, current, horsepower, and application duty.

What happens if a soft starter is undersized?

An undersized soft starter may overheat, trip during startup, fail to accelerate the motor, or suffer premature component failure. Sizing should always be based on motor full-load current, load type, and starting duty.

Can soft starters reduce voltage dips during motor startup?

Yes, soft starters can reduce voltage dips by limiting inrush current during acceleration. This helps reduce disturbances to other equipment connected to the same electrical system.