Galco will be closed Friday, July 3rd in observance of Independence Day.

Create or sign in to your account for the best pricing!

Your account pricing is now applied.

Toggle Nav
Search
My Cart

Capacitive Proximity

We can't find products matching the selection.

Industrial Capacitive Proximity Sensors for Non-Metal Detection and Level Sensing

Industrial capacitive proximity sensors detect targets by sensing changes in capacitance, which makes them a strong choice when you need non-contact detection of non-metallic materials. They are commonly used to detect plastics, wood, glass, paper, powders, pellets, and liquids, including through certain non-metal container walls depending on the sensor and application. In manufacturing and packaging environments, capacitive proximity sensors are often chosen for presence detection, part verification, and simple level sensing tasks where photoelectric or inductive sensing is not ideal.

For correct selection, start with the target material and how it will present to the sensor. Key considerations include sensing distance and repeatability, flush versus non-flush mounting, and whether the application involves moisture, dust, residue buildup, or temperature swings that can affect sensitivity. Many capacitive sensors include sensitivity adjustment, which can be useful for dialing in performance on challenging targets, but it also means you should plan for lockout, setup standards, and maintenance checks so settings do not drift over time. If you are comparing sensor types for a specific detection challenge, it can help to browse the broader sensors category to align the sensing principle with the environment and target.

Correct usage is largely about mounting and stability. Install the sensor rigidly to prevent vibration-induced changes, keep the sensing face clear of heavy buildup when possible, and route cables to avoid electrical noise issues in busy control cabinets. For level sensing in bins, hoppers, or tanks, confirm that the sensor is positioned to avoid false triggering from material flow patterns, condensation, or wall thickness variation. In applications where capacitive sensing may be influenced by changing material properties, you may also want to compare alternatives such as ultrasonic sensors, which can be better suited for certain distance and level applications depending on the surface conditions and required range.

Frequently Asked Questions

What can a capacitive proximity sensor detect that other proximity sensors cannot?

Capacitive proximity sensors can detect many non-metal materials, including plastics, wood, glass, powders, and liquids, which is a common limitation for inductive proximity sensors that primarily detect metal. That makes capacitive sensors useful for packaging lines, material handling, and basic level sensing where the "target" may be a non-conductive product or a liquid behind a non-metal wall. If you are evaluating the best sensing approach across your application, start with the broader sensors category and compare by target type and environment.

Which specs matter most when selecting an industrial capacitive proximity sensor?

Most selections come down to sensing distance, mounting style (flush or non-flush), output type and electrical compatibility with the control system, and environmental ratings appropriate for washdown, dust, oils, or temperature variation. It is also important to consider sensitivity adjustment and how stable you need detection to be when humidity or material composition changes. For applications that are primarily level sensing over a broader range, it can be worth comparing with ultrasonic sensors to see which technology better fits the operating conditions.

Why do capacitive sensors sometimes false trigger, and how can I reduce it?

False triggering is often caused by environmental factors that change capacitance near the sensing face, such as moisture, residue buildup, conductive dust, or gradual changes in the surrounding material. To reduce it, mount the sensor securely, keep the sensing face as clean as practical, follow recommended spacing from nearby metal and other sensors, and standardize sensitivity settings during commissioning so adjustments do not vary from machine to machine. If the environment is particularly challenging, reviewing alternative sensing technologies within sensors can help identify a more stable solution for the application.